User Activity

Hi people,The encoder failures can be detected by the timing unit. Transition errors can be found in encoder systems. A state diagram can be used to depict the reading on the two inputs, which equates to a 2-bit gray code. It is predicted that only o...
Hi People,I need to know what will happen when I forget to set the clock configuration by using system clock configuration function. Is there any default clock configuration will set in the microcontroller when I forget to set clock configuration?I'm...
I have configured the stm32wb with 247 data transmission but in the receiver side the buffer seems like it transferred only 20 bytes in the notification. For note: The values are updated in the 255 sized cmd_buffer in the aci_gatt_update_char_value(...
what is mfx?why the ADCLRCLK is connected to the mfx_gpio5?Is that codec device act like a master or slave for the given configurations?Please send me the results faster....
Kudos given to