2020-12-01 8:33 AM
I am trying to set up interrupt driven reading of X Y Z accelerations and X,Y and Z Gyro data on an ISM330DLCLSM6DSM. The plan is to generate an active high signal on INT2 when data becomes available as signalled by INT2_DRDY_XL (BIT0) of INT2_CTRL going high. The subsequent low to high voltage transition on the INT2 pad should then wake up an external microprocessor to process the sensor data.
Unfortunately my microprocessor never sees the interrupt so it never wakes up.
I am reasonably confident the microprocessor hardware is OK – I got your polling example (p26 of AN5125) to work fine.
I suspect there may be something missing from my register workflow. - see below
Would you have a look at my attempt which I have set out below, please?
REGISTER SET UP
System power up – wait 1 second
//Set up accelerometer ODR = 26Hz, low power and accel full scale
CTRL1_XL = 0x24
CTRL6_C = 0x10
//Set up gyro ODR = 26Hz, low power and gyro full scale
CTRL2_G = 0x24
CTRL7_G = 0x80
//Set up accelerometer data ready signal to appear on INT2 pad
INT2_CTRL = 0x01
//set up DRDY signal latched mode
DRDY_PULSE_CFG = 0x00
//set up BOOT normal, Block Data Update ON, H_LACTIVE active high, PUSH PULL, SIM 4wire //spi, IF INC on, BLE-LSB @lower address.
CTRL3_C = 0x44
//enable TIMESTAMP COUNT
CTRL10_C = 0x20
2020-12-01 9:44 AM
Hi @CHarr.1 ,
I would suggest you to consider the examples on Github for the LSM6DSM device, that show the configuration of the device for different applications.
/* Enable Block Data Update */
lsm6dsm_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
/* Set full scale */
lsm6dsm_xl_full_scale_set(&dev_ctx, LSM6DSM_2g);
lsm6dsm_gy_full_scale_set(&dev_ctx, LSM6DSM_2000dps);
/* Set Output Data Rate */
lsm6dsm_xl_data_rate_set(&dev_ctx, LSM6DSM_XL_ODR_12Hz5);
lsm6dsm_gy_data_rate_set(&dev_ctx, LSM6DSM_GY_ODR_12Hz5);
/* Enable drdy 75 μs pulse: uncomment if interrupt must be pulsed */
//lsm6dsm_data_ready_mode_set(&dev_ctx, LSM6DSM_DRDY_PULSED);
/* Enable interrupt generation on DRDY INT2 pin */
lsm6dsm_pin_int2_route_get(&dev_ctx, &int_2_reg);
int_2_reg.int2_drdy_g = PROPERTY_ENABLE;
int_2_reg.int2_drdy_xl = PROPERTY_ENABLE;
lsm6dsm_pin_int2_route_set(&dev_ctx, int_2_reg);Please let me know if it can be of your help.
-Eleon