MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unico-GUI tools bar - icons showing up on top of each other

Well, the Unico-GUI software was working fine, and one day all of the tools (bars, plot, data, etc) started getting drawn on top of one another, and the last one (pedometer) is the one on "top" and the only one I can now select. Any idea how to fix ...

0693W00000SucYeQAJ.png
Brian Rau by Associate III
  • 1696 Views
  • 3 replies
  • 0 kudos

LSM6DS0X STEP COUNT READ BUG

After loading a new decission tree for the Machine Learning Core the behaviour of the Step count registers of the pedometer changed.I must note that none of the code changed, just the register mapping corresponding the decision tree loaded to the MLC...

PPill.1 by Associate
  • 1096 Views
  • 1 replies
  • 0 kudos

LSM6DSO32 taking High Current

I have powered from LSM6DSO32 through a 3V Coin cell battery and connected with Nrf52810 using I2C.Without any coding sensor taking around 2mA and after flashing its taking 4MA.I am getting the readings correctly.Attached the schematics

0693W00000SttviQAB.png
V.Jose by Associate II
  • 1749 Views
  • 3 replies
  • 0 kudos

Step count is non-zero even though object is stationary (LIS2DS12)

Hello ST,I am using LIS2DS12 sensor for step detection application. I read the step count register every 1 minute and reset the count value. I observe that even if the object is stationary, the step count register has a non-zero value (The value vari...

AB.4 by Associate II
  • 2249 Views
  • 5 replies
  • 0 kudos

LSM6DSxx Gyro "Ringing"

I'm trying to use several different IMUs in the LSM6DS family (LSM6DSOX and LSM6DSO32). Both of them are exhibiting "ringing" on the three gyro axes when exposed to shock (knocking the PCB against a table). It almost looks like there's no anti-aliasi...

JimJ by Associate
  • 1621 Views
  • 1 replies
  • 0 kudos

the sensory library does not work at all.

Hello, I'm working on a project involving voice recognition. So, I used the stm32 sensory library to complete this project and the MP23DB02MM digital MEMS PDM microphone. However, I only found one example that used STM32H747I-DISCO, so I ported it to...

0693W00000SuITyQAN.png 0693W00000SuIToQAN.png 0693W00000SuIXCQA3.png

Read lsm6dso32 data via libiio

We are trying to use lsm6dso32 accelerometer/gyroscope connected to a custom hardware (non-st) via i2c. What we want to achieve is reading measured values continuously, ideally via libiio (buffered).We are building a custom linux (kernel version 5.4)...

NKuhn.1 by Associate II
  • 2454 Views
  • 3 replies
  • 0 kudos