MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STEVAL-BCN002V1マル�?センサ・ボードを使�?��?��?��?��?�。 https://www.st.com/ja/evaluation-tools/steval-bcn002v1b.html#overview

付属�?�プラスティックケース(丸型)を使�?��?��?��?��?��?��?��?開�?�る事�?��?��??�?��?�ん。開�?�方を教�?��?��??�?��?��?�。​

0693W00000Suzs3QAB.jpg
ROnod.1 by Associate
  • 1029 Views
  • 1 replies
  • 0 kudos

Resolved! I would like to use iis2dh to detect motor vibration with following use case. Is it possible to generate interrupt from deep sleep when vibration detected by iis2dh?

I would make the IoT device that detect vibration of the FAN. I will use this industrial portable blower FAN . https://www.indiamart.com/proddetail/portable-blower-fan-15055431262.htmlScenario1. To saving the energy of the device, the device goes to...

SSong.2 by Associate II
  • 1433 Views
  • 1 replies
  • 0 kudos

Why is there no 9-axis IMU available for ST now?

For absolute orientation estimation, magnetometer serves as an important role to calibrate the angle drift.However, it seems there is no 9-axis IMU available now.(ST LSM9D... is obsolete.)However, for low-cost, consuming purpose 9 axis IMU: BNO055 fo...

YCHEN.3 by Associate
  • 2859 Views
  • 1 replies
  • 3 kudos

Resolved! ABPDLNN100MG2A3 pressure sensor data manuplation

Hi all I am working on ABPDLNN100MG2A3 pressure sensor from honeywell which is an i2c communication, i have read the sensor data through i2c and saved it in two variable a and b the issue is how to convert the raw data to millibar, any thoughts kind...

NJP.1 by Associate III
  • 1758 Views
  • 1 replies
  • 0 kudos

Resolved! IIS3DWB Interrupt stops triggering while sampling for long periods

I have been using the IIS3DWB evaluation board alongside TIs CC1352P2 uC to bring up software ahead of the actual hardware arriving. The SPI bus speed is 8MHz in mode 3.The IIS3DWB is configured only sample accelerometer data on 3 axis and to store t...

0693W000007Dqr6QAC.jpg 0693W000007DqrLQAS.jpg
JDoug.1 by Associate II
  • 6247 Views
  • 10 replies
  • 0 kudos