MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to restore SensorTile.Box to factory defaults

I tried following this tutorial (https://community.st.com/s/question/0D50X0000BYnQt6/sensortilebox-not-connecting), but it looks like DfuSe is obsolete, and I should use the new STM32CubeProg tool. I couldn't seem to find any information on how to us...

LWang.7 by Associate
  • 6173 Views
  • 7 replies
  • 0 kudos

LSM6DSL marking meaning

Hi,I am using the LSM6DSL, i can see that the chip marking is different for some of my chips,some have SF 951 and others have 952. Further, I am getting different sensor results from each, Does someone know what is the difference between them?Thanks

GORDI by Associate
  • 2043 Views
  • 2 replies
  • 0 kudos

Tilt functionality based on Wakeup mechanism

Hello,We are working on tilt feature development based on LIS2DW12 sensor.For the development of the tilt feature with the help of Wakeup interrupt and following the attached example belowSo, How to set the sensitivity value from the open to the clos...

0693W00000QNynhQAD.png 0693W00000QNzQ0QAL.png
ChintaN1 by Associate III
  • 1112 Views
  • 1 replies
  • 0 kudos

lsm6dsr gyro output abnormal sometimes

Dear SIR,In my application is to use lsm6dsr gyro values.When the set is in stationary state, sometimes the X component gyro values become large that cause wrong calculation.It happens randomly and other sets not seen the case currently.I have no ide...

E-John by Associate III
  • 1139 Views
  • 0 replies
  • 0 kudos

LSM6DSO linear acceleration sensitivity tolerance

The datasheet for the LSM6DSO does not specify the tolerance of the linear acceleration sensitivity. Can you please tell me what the linear acceleration sensitivity tolerance is for this part.To be clear, I would expect to find offset and sensitivity...

RBarl.1 by Associate
  • 1263 Views
  • 1 replies
  • 0 kudos

LSM6DSL - which values should i get for position

hellowe are using LSM6DSL with full-scale acceleration range of ±2g. each one of x/y/z axis has 2 bytes output value: OUTX_L_XL (28h) + OUTX_H_XL (29h). as far as i understand, we should get 2^16=65,536 value for -2...+2g. i.e. 65,536/4=16,384 for 1g...

ABran.4 by Associate II
  • 3124 Views
  • 8 replies
  • 0 kudos