Skip to main content
RBarl.1
Visitor II
September 9, 2022
Question

LSM6DSO linear acceleration sensitivity tolerance

  • September 9, 2022
  • 1 reply
  • 883 views

The datasheet for the LSM6DSO does not specify the tolerance of the linear acceleration sensitivity. Can you please tell me what the linear acceleration sensitivity tolerance is for this part.

To be clear, I would expect to find offset and sensitivity accuracy/tolerance figures for linear acceleration and angular velocity:

* LA_TyOff: Linear Acceleration offset accuracy

* LA_So%: Linear Acceleration sensitivity tolerance

* G_TyOff: Angular Velocity offset accuracy

* G_So%: Angular Velocity sensitivity tolerance

The datasheet has three of these (LA_TyOff, G_TyOff and G_So%), but is missing LA_So%.

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    September 13, 2022

    Hi @Community member​ ,

    from characterization data, I can indicate you +-1% / +-2% as typical value for the LA_So% parameter.

    -Eleon