HelloWe must replace the old LSM6DS with the new one LSM6DOX because of End of Life of the first one.Checking the results on the same jig, reveals half of the Accelerometer part of the new chip. Do you have a detailed documentation which may support ...
I have Dell laptop with 4K display (XPS 15).A solution to handle this - to reduce the display resolution to 640x860 by the OS. please use updated JRE which can handle such displays.
Posted on July 08, 2018 at 21:35i have the st-link V2 (the old one), and I'm looking for the 4 connections it needed, in order to program my CPU. any idea or link to such info?
HIThere are actually two problems:The frequency response, which is lower in the new oneThe signal level of the 3 gyroscope axes is half the scale. You can clearly see it in the Z axis because of this specific recording but the 1:2 relation is also at...