MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DE12TR accelerometer component query

Hello,We are going to use LIS2DE12TR accelerometer, in our ultra low power device, to wake on motion. Here is schematic for LIS2DE12TR, Our requirement :1) ultra low power consumption2) Wake MCU on Motion by INT_1 Pin Below are queries regarding sche...

_legacyfs_online_stmicro_images_0693W00000bhdSSQAY.png
DBhut.1 by Senior
  • 1364 Views
  • 1 replies
  • 0 kudos

Resolved! ILPS22QS Cleaning After Soldering

TN0018 calls out in the Process considerations section that the board must be properly cleaned after soldering if "self-cleaning" solder paste is not used. Are there any guidelines on cleaning methods that will not damage the sensor? Can the sensor p...

DBass.2 by Associate
  • 1429 Views
  • 1 replies
  • 0 kudos

Resolved! DC bias from MEMS microphone using ADF on STM32U5

I have a MEMS microphone (IM72D128V01, using this eval kit) with PDM output connected to a STM32U5 NUCLEO board.It's connected to the ADF/Audo Digital Filter peripheral which I have configured to provide a 5th order CIC filter with a 32x decimation f...

DGran.3 by Associate II
  • 3662 Views
  • 3 replies
  • 0 kudos

Thermal response

One of the critical measurements for the analysis of bridges is the thermal response. The 201/109 combination has an average thermal response in the FFT of 1.5 milli-g - it is slightly frequency dependent, but ignoring that the standard deviation mea...

L3GD20 does not send the x y an z acceleration values

hello,I am using the L3GD20 to measure the angles, I have a 10 ms interrupt and in this interrupt service routine I read each time the 6 Output registers, I am configuring the gyro like this:GyroscopeDriver.TL3GD20_Reg_Struct.Who_Am_I = I_AM_L3GD20; ...

0693W00000aIUXFQA4.png 0693W00000aIUeBQAW.png

Simple procedures to sleep and wake-up lsm6dso

Hi, I'm trying to implement sleep and wake-up function in my project. I read the AN5192 Interrupt generation, but doesn't work. My project use nrf52832 with I2C and init my gyroscope/accelerometer following the procedure below: write_register(LSM6DS0...

LClad.1 by Associate II
  • 2088 Views
  • 1 replies
  • 0 kudos

How to change a network called in FP-AI-CTXAWARE1 package?

Hello, I recently bought the STEVAL-MKSBOX1V1 card (Sensortile.box). I would like to perform emotion recognition from speech through a convolutional network of my own creation. I downloaded the FP-AI-CTXAWARE1 package and opened the project on STM32 ...

FRana by Associate
  • 1724 Views
  • 1 replies
  • 0 kudos