cancel
Showing results for 
Search instead for 
Did you mean: 

How to enable the MLC option for the MKI197V1 in WL55?

hkout.1
Associate

Hello,

I'm trying to enable the MLC option for the MKI197V1 and I'm having some trouble.

The DatalogFusion runs fine when configured for the WL55JC, but what I want is the MLC option that can be seen on the DataLogExtended sample.

Any guidance is appreciated.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Miroslav BATEK
ST Employee

I think there are a few options but unfortunately none of them is quick and easy.

Option 1: Manually port DatalogExtended firmware which is available in X-CUBE-MEMS1 package to your board with WL55JC.

Option 2: Create your own firmware based on PID driver for LSM6DSOX which you can find here.

Option 3: Generate DatalogTerminal firmware using STM32CubeMX and X-CUBE-MEMS1 package and then add code working with MLC.