MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ILPS22QS addressing

Hi,In my project, I would like to connect multiple ILPS22QS pressure sensors (from 8 up to 256 units) to a single controller. I saw the dynamic addressing command supported by I3C ENTDAA. However, I also saw the provisional ID is not arbitrary. GETPI...

Jinhao by Associate II
  • 4862 Views
  • 6 replies
  • 4 kudos

Accelerometer calibration

Hi ST team,I would like to know if I need to calibrate my sensor or if you can tell me a method to validate my X, Y and Z outputs.I'm getting the following values in a test but how can I know if my method is correct? I was reading and at the current ...

TVela1_0-1692757896595.png TVela1_1-1692758309256.png
TVela.1 by Associate III
  • 1661 Views
  • 1 replies
  • 0 kudos

HSDatalog2 problem with STWINBX1

We are using the STEVAL-STWINBX1 at a CNC machine to gather vibration data. We are using the fp-sns-datalog2 HSDatalog Python framework to record the data over USB. Unfortunately, the data seems to always get corrupted in longer measurements (>5 min)...

nicolas_tudarmstadt_0-1692022911669.png

Resolved! Getting true north with the LIS2MDL and LSM6DSO sensors.

I use LIS2MDL and LSM6DSO sensors (with MotionMC and MotionEC libraries) for getting true north direction. I tested this configuration on IKS01A3 board and it works. But on my custom board, I'm having trouble with getting true north direction. After ...

_legacyfs_online_stmicro_images_0693W00000bl3Z1QAI.png _legacyfs_online_stmicro_images_0693W00000bl3ZBQAY.png
ALT.1 by Associate
  • 2572 Views
  • 2 replies
  • 0 kudos

Single and double tap on LSM6DSL

Posted on April 20, 2017 at 17:40Hi,I am using the LSM6DSL with a SMT32L476. My question is in relation to the single and double tap generated events (on INT2 pins).1�) When I single tap on the sensor I have an interruption on INT2. If I read TAP_SR...

Omnia . by Associate II
  • 1474 Views
  • 1 replies
  • 1 kudos

STWINKT 1B bug in fft analys demo.

In ultrasoun library has a bug. If change you in fft_app.h FFT_OUTPUT program is not compiled. Please change code like this  static void FFT_Thread(void const *argument) { (void) argument; #if (configUSE_APPLICATION_TASK_TAG == 1 && defined(TASK_F...