MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is there a reference platform available for ScanAR

Is there a reference platform available for ScanAR as mentioned here?https://www.st.com/content/st_com/en/about/innovation---technology/mems-scanar.htmlOur reference designAdditionally, to ensure a faster and a swifter integration cycle, ST develo"

NPete.3 by Associate
  • 1761 Views
  • 2 replies
  • 2 kudos

Couldn't initialize MotionCP library

I have connected X-Nucleo-IKS02A1 to Nucleo H563Zi.When I am trying to initialize the MotionCP library using MotionCP_Initialize() function, it is not getting initialized and I couldn't step into it.But when I initialize IKS02A1_MOTION_SENSOR_Init(IK...

Priyaa by Associate II
  • 1058 Views
  • 1 replies
  • 0 kudos

Sample code for IMU

Hi ST experts,Is there any sample codes available for IMU?I checked the info of X-Cube-MEMES-XT1 is already NRND.  

STLearner by Associate III
  • 3595 Views
  • 4 replies
  • 1 kudos

Resolved! LSM6DSV FSM example with baro (LPS22XX) as external sensor?

I have examined the FSM example folder on github and, while there is an example for an external magnetometer, I haven't found any examples for an external barometer. Is there such an example? And if so, where can I find it?I believe I can create my o...

KWine by Senior
  • 2848 Views
  • 4 replies
  • 0 kudos

Resolved! reading zeroes from IIS3DWB FIFO

Sometimes, I am reading zeroes from IIS3DWB FIFO. I thought maybe it is because I am using a protoboard (using MKI208) so I connected it directly (with cables) to RPi 4 but it still happens.I guess it is not normal to find these in FIFO, can it be du...

mete by Senior II
  • 1705 Views
  • 1 replies
  • 0 kudos

Resolved! asm330lhhx scale factor for each x, y, z axis

Hello,For the asm330lhhx device, when does the scale value change and get set?  I am trying to determine if the scale factor needs to be checked only once at power up or continually while reading the raw x, y, and z values for both the gyro and the a...

Resolved! LSM6DSV Sensor Hub current consumption?

Based on power measurements I infer that using the LSM6DSV embedded SensorHub with a single slave (LPS22DF) costs ~6.4 uA. I can't find the expected current consumption for the LSM6DSV Sensor Hub in the data sheet or application notes. Is this a reas...

KWine by Senior
  • 2427 Views
  • 3 replies
  • 0 kudos

Resolved! Documentation for MEMS module

Where can I find the proper documentation for the functions in X -Cube - MEMS package and clear explanations for the use of functions

Priyaa by Associate II
  • 1371 Views
  • 1 replies
  • 0 kudos