MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STHS34PF80 IR Sensor Performance in Continuous Mode

Hello,We are currently in the process of developing firmware for a device that contains the STHS34PF80 IR Sensor.At present, we have decided to use the continuous mode of this sensor, and we would like to seek clarification on its behavior under cert...

KD2 by Associate II
  • 8376 Views
  • 7 replies
  • 0 kudos

send motion sensor data via BLE with STEVAL-STWINKT1B

Hello!I am trying to create a program where I send motion sensor's data via BLE using evaluation board STEVAL-STWINKT1B. For that, I have used as a guide the firmware example on the board's website (https://www.st.com/en/embedded-software/stsw-stwink...

aag by Associate II
  • 3196 Views
  • 3 replies
  • 0 kudos

LSM6DSV SFLP 是否支持9轴融合?

我们现在正在调研LSM6DSV,确定他的SFLP支持6轴融合并可以正常输出四元数。我们想知道他是否支持9轴融合(+磁力传感器)?如果支持如何实现?

Yansu by Associate III
  • 1960 Views
  • 2 replies
  • 1 kudos

Log not stored in STEVAL-MKBOXPRO 's SD card.

Hi team,I used algo builder(Version 3.2.0.4544) and tried to store ACC ,Gyro and other sensor values in SD card. I can see the sensor values in User Messages window(Unicleo GUI), but that data not stored in SD card. Kindly help to store the data in S...

Daya_0-1701600938983.png
Daya by Associate II
  • 1530 Views
  • 1 replies
  • 0 kudos

How to get 6DOF from STVAL-MKBOXPRO

Hi all,                               Can we get 6DOF(Acc + Gyro only) quaternion (Game Rotation Vector) data from STVAL-MKBOXPRO?. Is there any example available? kindly share the link.

Daya by Associate II
  • 1190 Views
  • 1 replies
  • 0 kudos

Resolved! Lenses for STHS34PF80 IR Sensor

Hello,We are currently in the process of developing a device that contains the STHS34PF80 IR sensor. After study of the datasheet and conducting our own tests, we have found that the sensor reliably detects a person within a 4-meter range. However, f...

KD2 by Associate II
  • 1920 Views
  • 1 replies
  • 0 kudos

The STTS22 temperature sensor gives me back 0 °C

Hello everyone,after some time that I use the sensor, it gives me back a temperature value of 0 °C.I'm using a library taken from github that I adapted to work with the STM32F407 microcontroller (can't post the link).The sensor works well but sometim...

SSerg.4 by Associate III
  • 2229 Views
  • 3 replies
  • 0 kudos

Why doesn't the gyro value come out

Hi,I am using the LSM6DSO32X(in STEVAL-MKI197V1) sensor on the STEVAL-MKI109V3 board.There is no external sensor.I see and follow the Datasheet, but the Gyro Data does not come out and the external sensor value comes out.I used Easy Configuration in ...

sygo_0-1701306155478.png
sygo by Associate II
  • 2404 Views
  • 4 replies
  • 0 kudos