User Activity

I am currently using the LSM6DSO32X sensor on a custom board. I want to connect a custom board to the Unico GUI tool and utilize its features. Is it possible? If possible, how can I achieve that?thank you
Hi,I am using the LSM6DSO32X(in STEVAL-MKI197V1) sensor on the STEVAL-MKI109V3 board.There is no external sensor.I see and follow the Datasheet, but the Gyro Data does not come out and the external sensor value comes out.I used Easy Configuration in ...
I am using lsm6dso32x.An5629 Datasheet Section 8 FSM Configuration Example implemented only Accelerometer.I don't understand.It seems that you did not set what data(gyro or accel) you use with FSM, but I don't understand how it was used as an Acceler...
I used the lsm6dso32x_read_data_polling example and got the same result as above.(with SPI)Is this the correct value?And when I checked the values ​​using Unico GUI tool, I got the same values ​​as above.Although the values ​​are similar to the examp...
Hi,I am using LSM6DSO32X using SPI communication in TI AM2634 Chip.By default, I made a packet of Ctrl1_xl and Ctrl2_xl to 0x10b0 0x1110, and the Accel data and GYRO data were output.I saw Datasheet, but it's too hard to understand what each register...