Skip to main content
Associate
December 4, 2023
Question

send motion sensor data via BLE with STEVAL-STWINKT1B

  • December 4, 2023
  • 3 replies
  • 2249 views

Hello!

I am trying to create a program where I send motion sensor's data via BLE using evaluation board STEVAL-STWINKT1B. For that, I have used as a guide the firmware example on the board's website (https://www.st.com/en/embedded-software/stsw-stwinkt01.html#get-software -- using example project BLE-SampleApp). 

The problem I am having is that once I start to manipulate the example project (I need to work with motion sensors, not with environmental ones) I start getting a lot of errors I don't really understand. 

Anybody has a solution or has had a similar problem as I have? I just need a project that reads the motion sensors every XX ms and sends the raw data through BLE. The central device I am going to read the data from is a Raspberry Pi 4B (all the other options the firmware example has wouldn't be necessary).

Thank you!

This topic has been closed for replies.

3 replies

Visitor II
December 4, 2023

Is it possible for you to copy-paste the errors to this forum?

Explorer
December 4, 2023

For issues modifying the BLE-SampleApp example for motion sensor data on the STEVAL-STWINKT1B, consider checking documentation, reviewing error messages, analyzing code changes, verifying hardware connections, updating SDK/toolchain, utilizing debugging tools, and exploring other motion sensor integration projects for insights.

aagAuthor
Associate
December 5, 2023

First of all, thank you for your fast response!

Going back to the issue, I am quite stuck with the project I intend to do. I have downloaded the firmware example (on the link attached on the previous post) and have been trying to merge the projects BLE-SampleApp (sends environmental sensor's data through BLE) and Serial_DataLog (sends motion sensor's data throught serial port). 

 

First I tried attaching Serial-DataLog's files to the BLE-SampleApp but a lot of error ocurred when I tried using the motion sensors functions. I can't remember exactly what the errors were, but suddenly a lot of them appeared. I can remember that a lot of the errors were due to multiple definitions, when the functions were declared only once (the errors didn't have a lot of sense). 

 

Since I stayed stuck in that project a lot of time, I have tried doing something similar but the other way around: trying to introduce the BLE files and functions into the Serial-DataLog application. I had some errors because there were lots of files that I had to attach, but I have managed to build the project without errors. What I have done is leave the original project the same but introducing the BLE initializacion functions. 

 

The problem is that now that I initialize the BLE, the task manager fails and the program goes to an infinite loop, and I don't understand why or how I can introduce the BLE communication...

 

The functions I use to initialize the BLE are Init_BlueNRG_Stack() and Init_BlueNRG_Custom_Services(), and the program stays stuck here:

aag_0-1701780465670.png

Does anyboda have a solution? It is supposed to be simple changing the example codes and adapting it to your interests, but I don't see it simple at all. I have been reading lots of documentation but I only read documents refering to the exaples given, and not on how to modify the examples... 

Any solution will be much appreciated because I can't think of more solutions... 

Thank you!!