MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Issue with HTS221TR Sensor in the Presence of Product Projections

Hello everyone,I am an engineer at an EMS, and one of our clients has reported an issue related to the use of the HTS221TR sensor. Our client has observed that some of their boards, on which this sensor is mounted, have been exposed to projections of...

AxelH by Associate
  • 1492 Views
  • 2 replies
  • 1 kudos

LSM6DSO Sample Rate

Hello,I would like to increase the sample rate of a SparkFun LSM6DSO which is controlled by the ESP32 Thing Plus C microcontroller (I am using the Arduino IDE and said libraries).I tried using the function LSM6DSO::setAccelDataRate() and LSM6DSO::set...

ItaiS by Associate
  • 1534 Views
  • 1 replies
  • 0 kudos

Resolved! IMU sensor

Hi all, Is there any difference between LSM6DSV16x and LSM6DSV16xTR except the packaging?Thanks in advance.

Daya by Associate II
  • 7205 Views
  • 5 replies
  • 1 kudos

Resolved! MEMS IMP23ABSU microphone

Hi, is the sensitivity in the datasheet (-38 dBV +-1) normalized to 1 Pa (e.g. -38 dB re 1V/Pa)?

TomRett by Associate III
  • 1716 Views
  • 1 replies
  • 0 kudos

LSM6DSR self test

I saw there are self test related code in the driver.What's the purpose of self test and when do we need to do self test? Thanks,

KFCUBE by Associate II
  • 1301 Views
  • 1 replies
  • 0 kudos

Resolved! Multiple STHS34PF80 IR sensors nearby each other.

Can several STHS34PF80 IR sensors be used simultaneously, when placed not far from each other, say on the same PCB? If STHS34PF80 infrared sensors are completely passive devices, there should not be any limitations of the distance between them, even ...

aziubin by Associate II
  • 2087 Views
  • 1 replies
  • 1 kudos

Unit of measure for the MEMS IMP23ABSU microphone

Hello, i have searched for this information, but couldnt find it anywhere. Whats the unit of the measured of the MEMS IMP23ABSU mic? I have used the STEVAL-STWINKT1B with the FP-SNS-DATALOG1 from which i created several .csv files that i now need to ...

TomRett by Associate III
  • 11885 Views
  • 14 replies
  • 2 kudos

RMS velocity calculation from accelerometer data

Hello everyone. I'm working on a vibration sensor with RMS velocity output based on measurements from an accelerometer with +-16g maximum acceleration range. There is a simple equation for calculation RMS velocity range and that is : VRMS=Apeak/2*pi*...

MGolm.1 by Associate II
  • 8916 Views
  • 2 replies
  • 0 kudos