MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! lis2dw12

Hello,I'm currently working with a custom board designed to read digital values from an accelerometer, specifically from the OUT_X, OUT_Y, and OUT_Z registers. However, I've encountered an issue: despite the accelerometer being physically stable, I a...

image.png
sde c.1 by Senior II
  • 3333 Views
  • 4 replies
  • 1 kudos

BlueCoin入门套件

BlueCoin入门套件使用波束形成算法时,采样率能达到多少啊 

insist_66 by Associate II
  • 1903 Views
  • 3 replies
  • 0 kudos

Resolved! Reading any register from IIS3DWB sensor only yields 11111111

Hello,I have run into an unexpected problem when trying to read registers from the IIS3DWB sensor. The setup is attached in the picture. I am using an Arduino Uno R3 and an STEVAL MKI208V1 board. The code is fairly simple so I am not sure what is goi...

xl by Associate
  • 2095 Views
  • 2 replies
  • 0 kudos

MP34DT05-A randome noise

Hello ST community,I am unfortunately facing a problem with the MP34DT05-A MEMS microphone. I am using the DFSDM module to read in the microphone. Unfortunately, it happens again and again that extremely strong noise is added at a random time (see pi...

3a9e992e-2607-47a1-a37b-e0b8182a61b5.png
ChRegBrg by Associate II
  • 3232 Views
  • 4 replies
  • 3 kudos

AcousticBF

Can the AcousticBF beamforming algorithm from FP-AUD-SMARTMIC1 algorithm be used on the entry-level kit of BlueCoin board (STEVAL-BCNCS01V1) to achieve audio acquisition at a sampling rate of 48kHz?

insist_66 by Associate II
  • 2824 Views
  • 3 replies
  • 0 kudos

STHS34PF80 how to use Unicleo-GUI with custom board

Hi ST-Team,We want to use the STHS34PF80 for presence detection. I am not very familiar with the sensor, as a just watchedthe webinar about the sensor last Tuesday.I think a good way to check the capabilities of the sensor is the STM32 Open Developme...

andywild2 by Associate III
  • 3117 Views
  • 4 replies
  • 0 kudos

ISM330DLC gyro strange measured values

Dear ST Team,Greetings. I'm currently employing the ST ISM330DLC accelerometer and gyrometer in my application.I've noticed some unusual readings when the gyrometer is stationary, and I would like to inquire whether this is expected behavior.I've opt...

NSemrHomeInit_0-1701861141016.png

Resolved! LSM6DSV Gyro Standard deviation out of range

Hi, I developed lsm6dsv driver on Android CHRE framework. In Android CTS test, some items failed, the reason is "LSM6DSV Gyro Standard deviation out of range: stddev=(0.004091, 0.001167, 0.000378) (expected (0.003456, 0.003456, 0.003456))". How to fi...

lemon923 by Associate II
  • 3948 Views
  • 4 replies
  • 0 kudos

I3G4250DTR issues

We have been using I3G4250DTR for 5 years in our production parts. We have been noticing some recent issues with the I3G4250DTR in that some boards are not sending data (DRDY) at all, or the data is intermittent (less than the 100 Hz data rate). It i...

ClaudioI by Associate
  • 1025 Views
  • 1 replies
  • 0 kudos