cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DW12 Output Values

TVela.1
Associate III

Hi experts,

I am working with the LIS2DW12 accelerometer and the AN5038 document mentions the function to calculate the output values of the axis. 2g is mentioned, but what about 4g, 8g and 16g? Is the factor "4" the same for all scales?

TVela1_0-1690469523903.png

Thank you in advance.

Best regards,

Tania

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

For higher scales, multiply it by the additional gain.

4x: (mg) = (VALUE) / 4 * 0.244 * 2

 

8x: (mg) = (VALUE) / 4 * 0.244 * 4

16x: (mg) = (VALUE) / 4 * 0.244 * 8

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Super User

For higher scales, multiply it by the additional gain.

4x: (mg) = (VALUE) / 4 * 0.244 * 2

 

8x: (mg) = (VALUE) / 4 * 0.244 * 4

16x: (mg) = (VALUE) / 4 * 0.244 * 8

If you feel a post has answered your question, please click "Accept as Solution".
TVela.1
Associate III

Thank you!