MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ULP mode LSM6DS032 configuration procedure

Hi all,Been trying to use the ULP mode on LSM6DS032 with following steps.1. Setting XL to Power down mode by setting XL_ODR bits to 0b0000  of CTRL1_XL register.2. Set I3C_DISABLE to 1 of  register CTRL9_XL. // Not sure if this is necessary3. Power d...

bimalpaneru_0-1706512371883.png

LIS2DE12 not reaching current consumption said in datasheet

Hello,I'm evaluating the LIS2DE12 accelerometer by using the combination of STEVAL-MKI175V1 and STEVAL-MKI109V3 along a Power Profiler Kit II from Nordic Semiconductors for current measurement.Method of test:I removed the jumper that source VDD, brid...

sch0bert_5-1705418750414.png sch0bert_3-1705418520338.png sch0bert_6-1705419238154.png sch0bert_7-1705419302266.png
sch0bert by Associate III
  • 3268 Views
  • 4 replies
  • 0 kudos

ASM330lhh

Hi,I am working with ASM330lhh, connected to my linux device via i2c.in the sysfs i can see the device with the command  "ls -l /sys/bus/iio/devices/iio:device1/"  that return:total 0 -r--r--r-- 1 root root 4096 Mar 24 14:21 consumers -rw-r--r-- 1 ro...

Orenzv by Associate
  • 2634 Views
  • 2 replies
  • 1 kudos

I don't know how to use STEVAL-STWINMA2

I possese STEVAL-STWINMA2 with STEVAL-STWINKT1B for ultrasonic measurements. As a setup, we have attached STWINMA2 to STEVAL-STWINKT1B and installed a software "X-CUBE- MEMSMIC1". Then, we took measurements with using UltrasoundFFT.exe in the SW_exec...

D_Tomita by Associate
  • 1291 Views
  • 1 replies
  • 0 kudos

Resolved! Unicleo-GUI Start Problem

Hi everyone,I'm working on a project which we use nucleo401re board and IKS01A2 mems expansion board. I mounted IKS01A2 on 401RE board properly and load the datalogterminal.bin file into the microcontroller. After i start unicleo, it connects to the ...

N ORhan by Associate III
  • 3657 Views
  • 6 replies
  • 2 kudos

Resolved! ILPS28QSW o-ring

Hi,I'm having a hard time to find a supplier for an o-ring to get the ILPS28QSW sensor waterproof.In AN5937 ST mentioned they use an o-ring with: ID 1.8mm, thickness 0.5mm (see picture below)Does anyone here know any supplier who make these, or have ...

nibbler_0-1704796396318.png ILPS28QSW_size.png
nibbler by Associate
  • 2176 Views
  • 3 replies
  • 0 kudos

Unico_GUI Board Detection and Input Data Formatting

Hi all, I was just wondering if anyone had some insight into what the Unico-GUI is looking for to identify a board before it makes a connection. Is it simply looking for a specific formatting of serial output information or does it need to identify t...

ZoeTakacs by Associate II
  • 2086 Views
  • 3 replies
  • 1 kudos

Resolved! Testing accelerometer settings in controlled environment (LIS2DW12)

Hi, do you have any suggestion of a mechanical test bench setup to verify (/evaluate) the chosen accelerometer parameters? I'm working with an LIS2DW12, but I expect my question applies to all accelerometers:I have configured the accelerometer to sen...

CF3nXftw by Associate II
  • 3254 Views
  • 4 replies
  • 1 kudos

Resolved! STEVAL-MKI109V3 Doesn't Work and can't update

I just received the STEVAL-MKI109V3 kit and it appears to be useless so far.The Unico-GUI tool sees the main board but cannot see the sensor plugged into it. I measured the VDD_DUT and VDDDIO_DUT nets and there is no voltage. But maybe that is suppos...

kb9nate by Associate
  • 1480 Views
  • 1 replies
  • 0 kudos

False step counts in LSM6DSOX when travelling in vehicles.

Hi,We are using LSM6dsox for motion detection and as pedometer. The step counter value gets incremented when travelling in vehicles. FP_REJECTION and ADVANCE DETECTION is not enabled because the current consumption is very high when we enable the MLC...

VPrad.2 by Associate
  • 1160 Views
  • 1 replies
  • 0 kudos