MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

h3lis200dl consumes too much power.

When I used the IIC communication mode of h3lis200dl, I connected the 7th pin SDO directly to the ground. Since the SDO pin has a pull-up resistor inside, the current is too large (about 60uA). I would like to ask if there is an unopened register to ...

132.png
Phoenix1 by Associate
  • 1776 Views
  • 3 replies
  • 0 kudos

How to store/resotre calibration data?

I'm using lsm6dsv, and must calibrate IMU everytime after power on. Can I read calibration data once, and restore to IMU without calibration?

Yansu by Associate III
  • 1719 Views
  • 2 replies
  • 0 kudos

Read number of unread samples in FIFO - LIS2DW12

GreetingsI am working with the LIS2DW12 accelerometer and I am struggling to read from, and use the FIFO in single-conversion mode, using i2c. The chip is on a dev board which can only be used with i2c, and the INT1 or INT2 pins are not available for...

ZAIDS-S23 by Associate III
  • 3455 Views
  • 3 replies
  • 0 kudos

High Frequency Noise From STWINMA2A

Hello everyone,I am currently working with STWIN+STWINMA2A microphone array for ultrasonic signal processing. I use the firmware "AMicArray_Microphones_Streaming" and connect the board directly to my laptop as an USB microphone.However, the data suff...

xiaohangz_0-1704828877639.png xiaohangz_1-1704828956551.png

Resolved! IKS4A1 eCompass application with Unicleo-GUI

Hello, I am trying to test the e-compass application with the IKS4A1 connected to a Nucleo-F446 and Unicleo-GUI. The firmware of the Nucleo F446 was produced from Cube-MX following the "Getting started with the STMicroelectronics X-CUBE-MEMS1 softwar...

MRaff1_0-1706620923031.png
MRaff.1 by Associate III
  • 2406 Views
  • 2 replies
  • 1 kudos

LSM6DSM - Inquiry regarding 12-sec periodic noise

I have been experiencing a peculiar issue with the LSM6DSM sensor, where noise occurs at a 12-second interval. This phenomenon is consistent across multiple units and locations. Notably, the noise seems to affect only the Z-axis.Settings: with the AC...