User Activity

At the moment I am making an application for 3D sound detection, in which I am making use of the STEVAL-STWINKT1B and the STEVAL-STWINMAV1 microphone array (which I haven't used yet). I am just starting, and I can not understand the operation of the ...
Hello, I am writing because I am trying to make an APP similar to the one in this video, in the comments there is a link with more information of the video in which I understand that there is code that they used for this application, since they say i...
Hello good afternoon, I am starting to make an application with the sensortile.box very similar to "baby crying". I would like to ask if you have any information that can support me in this process, for example to activate the use of the AI folders i...
Hello could someone explain me for the FFT LINE COMPARE that is in the ST BLE SENSOR APP for the sensortile.box what are the parameters that appear to edit? and also for the FFT COMPARE, which I understand that it will be the same and the "Name file ...
I'm trying to do a program like a baby crying and i'm looking for the code of babycrying program. I need to do a program that detects unwanted noises in cars, so i think that maybe is similar than the babycrying app.I thought it was possible using th...
Kudos given to