MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why doesn't the gyro value come out

Hi,I am using the LSM6DSO32X(in STEVAL-MKI197V1) sensor on the STEVAL-MKI109V3 board.There is no external sensor.I see and follow the Datasheet, but the Gyro Data does not come out and the external sensor value comes out.I used Easy Configuration in ...

sygo_0-1701306155478.png
sygo by Associate II
  • 1196 Views
  • 4 replies
  • 0 kudos

LSM6DSO Sample Rate

Hello,I would like to increase the sample rate of a SparkFun LSM6DSO which is controlled by the ESP32 Thing Plus C microcontroller (I am using the Arduino IDE and said libraries).I tried using the function LSM6DSO::setAccelDataRate() and LSM6DSO::set...

ItaiS by Associate
  • 886 Views
  • 1 replies
  • 0 kudos

Resolved! IMU sensor

Hi all, Is there any difference between LSM6DSV16x and LSM6DSV16xTR except the packaging?Thanks in advance.

Daya by Associate II
  • 5178 Views
  • 5 replies
  • 1 kudos

LSM6DSR self test

I saw there are self test related code in the driver.What's the purpose of self test and when do we need to do self test? Thanks,

KFCUBE by Associate II
  • 751 Views
  • 1 replies
  • 0 kudos

Resolved! Multiple STHS34PF80 IR sensors nearby each other.

Can several STHS34PF80 IR sensors be used simultaneously, when placed not far from each other, say on the same PCB? If STHS34PF80 infrared sensors are completely passive devices, there should not be any limitations of the distance between them, even ...

aziubin by Associate II
  • 1498 Views
  • 1 replies
  • 1 kudos

Unit of measure for the MEMS IMP23ABSU microphone

Hello, i have searched for this information, but couldnt find it anywhere. Whats the unit of the measured of the MEMS IMP23ABSU mic? I have used the STEVAL-STWINKT1B with the FP-SNS-DATALOG1 from which i created several .csv files that i now need to ...

TomRett by Associate III
  • 5706 Views
  • 14 replies
  • 2 kudos