MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM9DS1 SDO always 0

Hey folks,I've fabricated a little PCB to glue an LSM9DS1 to an ESP32-S3. As far as I can see, the ESP32 is sending the correct signals but the LSM9DS1 isn't returning anything useful. Here's what I get when I try to read 0x0F, the WHOAMI register, f...

SDS00014.png Untitled.jpg SCH_Adafruit LSM9DS1 Rev A_1_1-Adafruit LSM9DS1 Rev A_1_2023-12-02.png

send motion sensor data via BLE with STEVAL-STWINKT1B

Hello!I am trying to create a program where I send motion sensor's data via BLE using evaluation board STEVAL-STWINKT1B. For that, I have used as a guide the firmware example on the board's website (https://www.st.com/en/embedded-software/stsw-stwink...

aag by Associate II
  • 2054 Views
  • 3 replies
  • 0 kudos

LSM6DSV SFLP 是否支持9轴融合?

我们现在正在调研LSM6DSV,确定他的SFLP支持6轴融合并可以正常输出四元数。我们想知道他是否支持9轴融合(+磁力传感器)?如果支持如何实现?

Yansu by Associate III
  • 1020 Views
  • 2 replies
  • 1 kudos

Log not stored in STEVAL-MKBOXPRO 's SD card.

Hi team,I used algo builder(Version 3.2.0.4544) and tried to store ACC ,Gyro and other sensor values in SD card. I can see the sensor values in User Messages window(Unicleo GUI), but that data not stored in SD card. Kindly help to store the data in S...

Daya_0-1701600938983.png
Daya by Associate II
  • 849 Views
  • 1 replies
  • 0 kudos

How to get 6DOF from STVAL-MKBOXPRO

Hi all,                               Can we get 6DOF(Acc + Gyro only) quaternion (Game Rotation Vector) data from STVAL-MKBOXPRO?. Is there any example available? kindly share the link.

Daya by Associate II
  • 782 Views
  • 1 replies
  • 0 kudos

Resolved! Lenses for STHS34PF80 IR Sensor

Hello,We are currently in the process of developing a device that contains the STHS34PF80 IR sensor. After study of the datasheet and conducting our own tests, we have found that the sensor reliably detects a person within a 4-meter range. However, f...

KD2 by Associate II
  • 1337 Views
  • 1 replies
  • 0 kudos

The STTS22 temperature sensor gives me back 0 °C

Hello everyone,after some time that I use the sensor, it gives me back a temperature value of 0 °C.I'm using a library taken from github that I adapted to work with the STM32F407 microcontroller (can't post the link).The sensor works well but sometim...

SSerg.4 by Associate III
  • 1294 Views
  • 3 replies
  • 0 kudos