cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple STHS34PF80 IR sensors nearby each other.

aziubin
Associate II

Can several STHS34PF80 IR sensors be used simultaneously, when placed not far from each other, say on the same PCB? If STHS34PF80 infrared sensors are completely passive devices, there should not be any limitations of the distance between them, even if their fields of view are intersecting, right?

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Correct, the STHS34PF80 are purely passive components and can be positioned directly next to each other without any problems and without any mutual interference.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Correct, the STHS34PF80 are purely passive components and can be positioned directly next to each other without any problems and without any mutual interference.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.