MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Typo in DS13431 - Rev 3 (ILPS22QS datasheet)

Hi,There is a typo in in the datasheet of the ILPS22QS datasheet: DS13431 - Rev 3.Table 19 on page 32 states that default value of CTRL_REG2 is 00h.But on page 39, chapter 9.7 CTRL_REG2 bit EN_LPFP has a default value of 1 resulting in 10h  I hope th...

Girardey_1-1705351034907.png Girardey_2-1705351161928.png
Girardey by Associate
  • 760 Views
  • 1 replies
  • 1 kudos

Resolved! lsm6dsr sensor motion information

Hello everyone, I am working with the lsm6dsr sensor. How can I solve the position information or how much I move with this sensor? I am looking at projects with examples on github, but I could not find how to solve the directions, how much the senso...

LSM6DSOX Example

Hi, I'm developing a project with a NUCLEO-WB55RG and I need to to communicate with a STEVAL-MKI197V1. I'm using the CUBE IDE v1.13.1 and the X-CUBE-MEMS1 v10.0.0. But I'm having a problem when trying to initiate the library calling LSM6DSOX_Init fun...

BMA400 library/example for STM32

Hi everyone,Is there a library or example of the BMA400 connected to an STM32 by I2C. There are very complete libraries but only for Arduino.Thank you!

grf14 by Associate
  • 2014 Views
  • 2 replies
  • 1 kudos

h3lis200dl power-down mode

Posted on March 19, 2018 at 11:51Hi,we are facing a problem to shut down h3lis200dl in our design. VDD is connected to VDD_IO and power is always connected to 3V battery (even when device is turned off). We are using SPI-communication and reading/se...

0690X0000060AA5QAM.png
Olov H by Associate
  • 1039 Views
  • 4 replies
  • 0 kudos

Resolved! LSM6DSOX INT1 & INT2 Trigger on Tap Detection

Hi,I have designed a circuit with the LSM6SDOX.It is operating via the I2C BUS and the Gyroscope and Accelerometer are sending data. I have also managed to configure Single and Double Tap detection, however it is the tap detection where I have an iss...

INT1 and INT2.PNG

Resolved! LSM6DSO sensor hub questions

Hi, I would like to ask for some clarification about LSM6DSO's sensor hub features.1. I am considering mode 2 to connect two sensors to LSM6DSO and LSM6DSO will communicate with MCU in i2c interface. In this case, when connecting two sensors, say LI2...

el659_0-1705055014758.png el659_1-1705055397228.png
el659 by Associate III
  • 1101 Views
  • 1 replies
  • 1 kudos

Resolved! LIS3MDLTR Part Marking

Hello, I am looking for a part marking for LIS3MDLTR. The part says SF 233, but am unsure if this is the correct marking. I have read ST does not post their part markings externally.