Self test in IIS3DWB
What is self-test in IIS3DWB and what is the criteria to indicate pass or fail??
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
What is self-test in IIS3DWB and what is the criteria to indicate pass or fail??
Hi @Federica Bossi , I need help with setting LSM6DSO sensor hub i2c master clock speed. How do I set the master i2c clock speed between LSM6DSO and external sensor for sensor hub operation? Is there registers or something else on LSM6DSO that contro...
HiWhat is the cut-off frequency of the analog anti-aliasing filter in the ISM330IS?RegardsChristoffer Brodersen
Hello,I have question please, can you tell me the protection index (IP) of the LPS28DFW ? also the LPS22DF has 22000g High shock survivability, it's perfromant for my application but for the LPS28DFW i don't find any information on the datasheet abou...
Hello,Please, for a pressure measurement in an environment of dust and humidity, which sensor between the 2 you recommend as well as what is the IP protection rating of each sensor.Thanks in advance
Hi,I am using the Lis2dh12 mems accelerometer sensor in a design. I configured it for a g-force threshold within any of the 3 axes and using the interrupt (pin 1) with the stream to fifo setting. I am using the I2c (400kbps) and ODR is 100 hz. When t...
I have performed the self-test on LSM6DSL and observed that it was noted the thresholds mentioned in the datasheet I want to know how these values of 90mg > xxx < 170mg & 150 dps> xxx <700dps measured?Why does the acceleration and gyro change when ...
Hi all, I'm trying to get some accurate orientation data from the accelerometer and gyroscopic capabilities of the LSM6DSV16X, but am getting some different data from different GUI software. The Unicleo-GUI paired with the STEVAL-MKBOXPRO (SensorTile...
Hi,I am using steval MKI160V1 coupled with pybv1.0 under microphyton (spi speed 525000bits/s).I'd like to get every samples from gyro and accel at 1666 hertz speed using interruption.I have configured lsm6ds3( whoami = 69h) to do so, but while I am f...
As shematic below the pin7 is connected to GND so there will be a 60uA leakage .so how to disable the internal pull up by config the register.