ST tile box pro sampling time issue
Hi all , I have stored IMU quaternion data into the SD card. I did use the Algo builder tool for that. I couldn't get the samples in configured 100Hz. Kindly help to store all samples in 100hz rate.
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi all , I have stored IMU quaternion data into the SD card. I did use the Algo builder tool for that. I couldn't get the samples in configured 100Hz. Kindly help to store all samples in 100hz rate.
Good dayI am using LSM6DSO with 3V3 VDD and 1V8 VDDIO.Can the supplies(VDD and VDDIO) be ON/OFF independently or is there a requirement for one of the two to be ON before the other?In my instance the VDD might come on before the VDDIO and in other ci...
Hi All,I started with example to make STHS34PF80 presence detection working.Now I tried to add effective presence detection range.Where should I start ? Is there a suggested process ?
Hi, I need clarification about interrupt on ILPS22QS barometric pressure sensor.My test project involves LIS3MDL and ILPS22QS connected to MSDA and MSCL on LSM6SDO, which is connected to an mcu in 4-wire SPI interface, to use sensor hub on LSM6DSO (I...
Is it possible to configure the LIS2DH12 so that it can receive a clock from the host (master) instead of the clock being generated by the LIS2DH12? I'm looking a the quality of the LIS2DH generated clock and it is spectrally not pure and has a sign...
Hello,I have STEVAL-MKI236A (ASM330LHB - IMU) evaluation board, How can I make use of the UNICO-GUI to interface with the board. I do see the board listed on the GUI but how will I be able to interface with gui with just I2C without using the MOTHERB...
Hi. I used LIS2DU12TR accelerometer IC on the PCB. It's angle value was changing every sec. but my smart phone app indicated current angle is 0.0 degree. current angle is -0.515648[proc_bt_read_all] TX data (len=15)00 00 02 00 00 00 00 00 00 7F...
I want to calculate the displacement using the MotionX library with the LSM6DSR sensor on the stm32. For example, I want to write a code that calculates the displacement when the sensor moves 20 cm to the right on the table or calculates the displace...
When I used the IIC communication mode of h3lis200dl, I connected the 7th pin SDO directly to the ground. Since the SDO pin has a pull-up resistor inside, the current is too large (about 60uA). I would like to ask if there is an unopened register to ...
I'm using lsm6dsv, and must calibrate IMU everytime after power on. Can I read calibration data once, and restore to IMU without calibration?