cancel
Showing results for 
Search instead for 
Did you mean: 

Using STEVAL-MKI236A with UNICO GUI

govindrzook
Associate II

Hello,

I have STEVAL-MKI236A (ASM330LHB - IMU) evaluation board, How can I make use of the UNICO-GUI to interface with the board. I do see the board listed on the GUI but how will I be able to interface with gui with just I2C without using the MOTHERBOARDs.

Thanks!

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Federica Bossi
ST Employee

Hi @govindrzook ,

Are you using the STEVAL MKI109V3?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hello @Federica Bossi 
I am not making use of STEVAL-MKI109V3 motherboard and currently directly using the evaluation board via SCL, SDA pins of I2C interface. is it possible to make use of the UNICO-gui without that motherboard?

Please advise thanks!

Federica Bossi
ST Employee

Hi @govindrzook ,

Yes, as explained in our official page, it is available for three operating systems: STSW-MKI109L for Linux Debian-based; STSW-MKI109M for Mac OS X; STSW-MKI109W for Windows. 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.