cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSO VDD and VDDIO sequencing and dependancy

AWolf.3
Associate

Good day

I am using LSM6DSO with 3V3 VDD and 1V8 VDDIO.

Can the supplies(VDD and VDDIO) be ON/OFF independently or is there a requirement for one of the two to be ON before the other?

In my instance the VDD might come on before the VDDIO and in other circumstance the VDD might be switched OFF and VDDIO might remain ON.

The device functions in I2C mode. Does CS have to be HIGH when VDD is applied or can CS be changed/set dynamically after VDD was applied?

Would this pose a problem?

Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @AWolf.3 ,

VDD and VDDIO can be ON/OFF independently.

In I2C mode the CS have to be high but, contrary to what you wrote, it is preferable to be connected to the VDDIO.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @AWolf.3 ,

VDD and VDDIO can be ON/OFF independently.

In I2C mode the CS have to be high but, contrary to what you wrote, it is preferable to be connected to the VDDIO.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.