MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Read number of unread samples in FIFO - LIS2DW12

GreetingsI am working with the LIS2DW12 accelerometer and I am struggling to read from, and use the FIFO in single-conversion mode, using i2c. The chip is on a dev board which can only be used with i2c, and the INT1 or INT2 pins are not available for...

ZAIDS-S23 by Associate III
  • 2409 Views
  • 3 replies
  • 0 kudos

High Frequency Noise From STWINMA2A

Hello everyone,I am currently working with STWIN+STWINMA2A microphone array for ultrasonic signal processing. I use the firmware "AMicArray_Microphones_Streaming" and connect the board directly to my laptop as an USB microphone.However, the data suff...

xiaohangz_0-1704828877639.png xiaohangz_1-1704828956551.png

Resolved! IKS4A1 eCompass application with Unicleo-GUI

Hello, I am trying to test the e-compass application with the IKS4A1 connected to a Nucleo-F446 and Unicleo-GUI. The firmware of the Nucleo F446 was produced from Cube-MX following the "Getting started with the STMicroelectronics X-CUBE-MEMS1 softwar...

MRaff1_0-1706620923031.png
MRaff.1 by Associate III
  • 1480 Views
  • 2 replies
  • 1 kudos

LSM6DSM - Inquiry regarding 12-sec periodic noise

I have been experiencing a peculiar issue with the LSM6DSM sensor, where noise occurs at a 12-second interval. This phenomenon is consistent across multiple units and locations. Notably, the noise seems to affect only the Z-axis.Settings: with the AC...

Resolved! How to effectively use lis2dw12 to detect motionless event ?

Hi All,I need a mechanism to detect motionless for 10s to make device enter power saving mode.For lis2dh12, I can use HPF with low x,y,z threshold and duration to detect an event that motionless for 10s.However I need more low power accelerometer lis...

SLin.11 by Associate III
  • 2431 Views
  • 6 replies
  • 0 kudos

Resolved! LIS2DW12 FIFO overflows upon wake-up by interrupt

GreetingsI have configured  the LIS2DW12, via SPI,  to sample and store samples, given the FIFO (configured in continuous mode) on a wakeup interrupt to INT1. The sensor, given its current configuration is able to wake up and sample but there is a wo...

ZAIDS-S23 by Associate III
  • 1447 Views
  • 4 replies
  • 0 kudos