MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! issue with NRF24L01 on STM32F07VET6 blackboard

I've been trying to interface the STM32F407VET6 with the NRF24L01 modules, however after trying multiple boards modules and library's it still fails to work. im not sure the issue is with hardware as ive tried multiple modules and the black board has...

voxe by Associate II
  • 2145 Views
  • 1 replies
  • 0 kudos

IKS02A1 and Nucleo H503RB don't work

Hi, I am curretly using a Nucleo H503RB and the IKS02A1 expansion board in order to use the ISM330DHCX.I tried several way to use via STM32Cube IDE which is my goal as i want to use C language without success to see any sign of an i2c adress with an ...

matkergo by Associate
  • 1801 Views
  • 1 replies
  • 0 kudos

How can I make BLE work on STWINKT1?

Hi,I am trying to use the BLE (SPBTLE-1S chip) on my STEVAL-STWINKT1 board. The idea was to use a project example from X-Cube-BLE2 with the following configuration :HCI_TL : BasicHCI_TL_Interface : UserBoardApplication : SampleAppI used the SPI2 to c...

KaisBo7 by Associate II
  • 2025 Views
  • 3 replies
  • 0 kudos

IIS2DLPCTR Internal LDO

I am thinking of powering the IIS2DLPCTR accelerometer VDD rail from a buck converter and wanted to understand if this part uses an internal LDO to step the VDD voltage down to power the internal MEMS block and ADC? Or does it use the supplied VDD di...

NBerr.1 by Associate II
  • 1224 Views
  • 1 replies
  • 0 kudos

SensorTile.Box PRO asks Bluetooth Code

When I connnect sensorTile.box from App.the followign msg poped ip continuously. and no fucntion work properlywhat is the reason. I upgraded the FW on FOTA  at the first connection.what is the suggestion ?Thanks!Forest  

forestxu_0-1718761080315.png
forest xu by Associate II
  • 2498 Views
  • 5 replies
  • 0 kudos

ML implementation in ISPU

Can anyone provide a documentation over integration custom ml algorithm in ISPU.If I have a machine learning model like tflite or onnx how can I deploy it in ISPU

Amith_lal by Associate III
  • 2254 Views
  • 3 replies
  • 2 kudos

ISM330DLC Low Power Mode

Trying to get the lowest power out of this device, but it seems to draw at least 900uA of current when even the accel and gyro are disabled. Any suggestions on how to get the current draw of this device lower? Here's my setup:Custom PCBnormal current...

NSmit.9 by Associate II
  • 2225 Views
  • 3 replies
  • 0 kudos

STEVAL-MKBOXPRO firmware that is compatible with ISPU dil24

I'm trying to make a demo with the ispu chip ism330is and the STEVAL-MKBOXPRO the issue is I can't find a suitable firmware for the tilebox pro that is compatible with the ispu and allows me upload the compiled UCF program into the chip. Below is a s...

benx1326 by Associate II
  • 1804 Views
  • 1 replies
  • 0 kudos

Unicleo gui not detecting IKSO1A2

Hello, I'm learning how to use stm32 hardware and how to program it and today i connect the X-NUCLEO-IKO1A2 to my board (Nucleo-GO71RB) and installed the inucleo software,  i did everythink like te st video said, but for some reason the software does...

Fxpires by Associate
  • 1647 Views
  • 2 replies
  • 0 kudos