MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH工作模式问题

我想知道LIS3DH的三种工作模式是什么?我收到了两份文件,一份是高分辨率模式、正常模式和低功耗模式,另一份是关机模式、正常模式和低功耗模式。我比较了两种模式的寄存器配置。低功耗模式相同,第一个数据中的高分辨率模式与第二个数据中的正常模式相对应。你能给我一个关于这个问题的具体解释吗?

LSM6DSO timestamp for external sensor event

Hi @Federica Bossi , I have a question about timestamp and the external sensor event.According to the application note of LSM6DSO (image above), timestamp's register is written when main sensor or external sensor event occurs. I have no problem with ...

el659_0-1717492879373.png
el659 by Associate III
  • 1478 Views
  • 1 replies
  • 0 kudos

I3G4250D Read the temperature

Hello,I am using a I3G4250D gyroscope and would like read the temperature. Currently, I read 246 (in decimal) in my register 0x26.In two's complement, it is equivalent to -9.   Then I have to multiply by -1 so -9 * -1 = 9°C (I am not sure)But It is t...

TomBr_0-1718294480109.png TomBr_1-1718294511992.png
TomBr by Associate II
  • 1928 Views
  • 2 replies
  • 0 kudos

Issue with MotionDI library initialization

I have added Digital Inclinometer application of X-Cube-MEMS1(9.6.0) on stm32f777zit6 wherein I want to read the rotation(angle) from LSM6DSL device. I have added all the required component files and Motion_DI library to the workspace.Reference taken...

Alps by Associate
  • 1339 Views
  • 1 replies
  • 0 kudos

Output Data Error for lsm6ds3tr-c

would you please help to review the attached log and give some advice to customer?Thanks.Attached is the test log data, test conditions:1. The device is fixed on the desktop without moving or shaking. 2.2. The CPU reads the X/Y/Z data of the Sensor v...

Vulnerability of LPS28DFW in hot humidified gas

I am measuring pressure using the LPS28DFW under conditions where the gas flow is approximately 70°C with a relative humidity of 80-100%. During measurement under these conditions, I encountered an issue where the sensor stops working. However, the s...

LIS322 by Associate
  • 1568 Views
  • 1 replies
  • 0 kudos

Accelerometer and gyroscope reading using sensor

Hi,I want to know the best solution to read accelerometer and gyroscope data using the STEVAL-MKI182V2 board with the STEVAL-MKI109V3. At this moment, I can use Unico-GUI to read live all the data from the sensor, but I want to make a AI model to rea...

unable to connect STEVAL MKBOXPROA to mems studio

Hi,I'm unable to connect my STEVAL MKBOXPROA  (SensorTile.Box Pro) to Mems Studio, here's what I get:"board not identified" I tried uploading the DataLogExtended.bin, and it says it programs successfully, but I noticed there's a quick "verification f...

Keef_0-1718150019155.png Keef_2-1718150133684.png
Keef by Associate II
  • 2305 Views
  • 3 replies
  • 0 kudos