cancel
Showing results for 
Search instead for 
Did you mean: 

Actual Detection Range and FOV of STHS34PF80?

mobaid
Associate II

Hello everyone,

I’ve been working with the STHS34PF80 sensor and would appreciate some insights regarding its detection range and field of view (FOV). In my tests, I’ve observed that the sensor detects presence effectively up to a range of about 1 meter when I set the presence threshold to 100 LSB. Additionally, the FOV seems to be around 30 degrees.

I’m wondering if these results align with what others have experienced. Is this the typical range and FOV for this sensor under similar conditions, or could there be some optimization or calibration that I’m missing? Any feedback or suggestions would be greatly appreciated!

Thanks in advance!

 

Note

sensor config:

lpf_m: 04, lpf_p: 04, lpf_p_m: 02, lpf_a_t: 00

sths34pf80_gain_mode_get 7
sths34pf80_tobject_sensitivity_get 2000
sths34pf80_odr_get 8
sths34pf80_block_data_update_get 1
sths34pf80_one_shot_get 0
sths34pf80_presence_abs_value_get 1
sths34pf80_tobject_algo_compensation_get 1
sths34pf80_presence_hysteresis_get 25
sths34pf80_motion_hysteresis_get 25
sths34pf80_tambient_shock_threshold_get 10
sths34pf80_motion_threshold_get 100
sths34pf80_presence_threshold_get 150

 

3 REPLIES 3
Federica Bossi
ST Employee

Hi @mobaid ,

We see no problem in the used configuration.

The expected FOV and detection range are much larger.

Can you give us more information about the test environment and conditions?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @Federica Bossi ,
Here are the test environment conditions :

 

T ambient

23’C ~ 25’C (Air conditioner)

Application

Indoor office

Sensor to Wall distance

3m

Sensor Hight

1m

Lens

N/A

AVG_TMOS : Number of averaged samples for object temperature

32

AVG_T : Number of averaged samples for ambient temperature

8

Interrupt source

Presence

Presence and motion detection setting

Presence threshold

150

Presence hysteresis

25

Motion threshold

100

Motion hysteresis

25

 

Thank you .

 

 

Subject: STHS34PF80 Sensor — Inconsistent Output with ESP32 and SparkFun Library

I am using the STHS34PF80 sensor (SparkFun Presence Sensor - STHS34PF80) with an ESP32 in my ceiling fan to automatically turn the fan ON and OFF based on human presence and motion. I’m using the official SparkFun library to read the sensor values.

However, I’m noticing inconsistent readings:

  • Sometimes the sensor gives values above 1000 when a person is around 60–70 cm away.

  • Other times, under the same conditions, it gives 0 or even negative values.

I would like to know:

  1. How can I configure the sensor for more reliable presence detection?

  2. Does the sensor have a refresh rate, integration time, or filtering option that needs adjustment in code?

Any guidance on how to stabilize or interpret the sensor output would be appreciated.

Thanks!