cancel
Showing results for 
Search instead for 
Did you mean: 

Can the LPS27HHW be used to detect non-water liquids, such as oil?

TIENHUA
Associate III

Hi Sir,

 

Can the LPS27HHW be used to detect non-water liquids, such as oil?

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @TIENHUA ,

Theoretically it is possible to see other liquid respect to water. The only issue is due to chemical material is present into the liquid you are referring. This can cause a damage of the gel present in the device. In case of some particles passes the gel, the device doesn't work properly. The suggestion is to test the device in desired liquid.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @TIENHUA ,

Theoretically it is possible to see other liquid respect to water. The only issue is due to chemical material is present into the liquid you are referring. This can cause a damage of the gel present in the device. In case of some particles passes the gel, the device doesn't work properly. The suggestion is to test the device in desired liquid.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.