User Activity

Hi Sir,I am reviewing the application schematic of the STUSB1600 in a dual-role Type-C design. I understand that when STUSB1600 operates as a Source, the output current can be configured through the CC_CAPABILITY_CTRL register.However, I did not see ...
What's the max current of the mosfet in the L6924D?We want to use AC adaptor to charge the battery and supply the system loading at the same time. So, we want to know the max current of power mosfet.Thank you. 
From the datasheet and AN4870, we understand that it is necessary to calculate the battery's internal impedance and measure the OCV table.After configuring CC_CNF and REG_VM_CNF, the STC3117 operates properly using its algorithm.The operating tempera...
Hi Sir, What internal adjustments have been made to cause the noise density to differ between the high-performance, normal, and low power modes of the ISM330DHCX? Filter? Gain?Thank you.
Hi Sir, Could you share the equation of current limit?I cannot find the related equation in the datasheet.Thank you.
Kudos from
Kudos given to