MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reading SFLP Data from ism330bx

I'm trying to extract the data Game Rotation Data from the ism330bx sensor. I'm just not quite sure, which setting to use for that. What I did so far:Setting the sensor for an ODR of 480Hz with a range of 4000dps and 8g.(ism330bx_reset(NULL)) (ism330...

ritzmo93 by Associate
  • 103 Views
  • 1 replies
  • 0 kudos

Mems configuration on Custom Board

Hello,     after experimenting MEMS sensors with the IKS4A1, I developed a custom board based on STM32F407 CPU with the LSM6DSV16XTR accelerometer+gyroscope and LIS2MDLTR magnetometer.The aim is to get board inclination and compass information with t...

MRaff.1 by Associate III
  • 130 Views
  • 1 replies
  • 0 kudos

Resolved! Implementation for MEMS1 librairi : don't work !

Hi,i am using ism330dhcx and lis2mdl on my custom board,i am able to configure and read data from accelero, gyro and magneto.i started the implementation of X-Cube-MEMS1 lib.when i compile the code, every thing is ok,but after running, when a functio...

malarab_0-1724321994996.png malarab_1-1724322019406.png malarab_2-1724322046678.png malarab_3-1724322172683.png
malarab by Senior II
  • 147 Views
  • 1 replies
  • 1 kudos

X-CUBE-MEMS1 application Inclinometer and eCompass

Hello,      on a custom board which mounts STM32F407 CPU with LSM6DSV16XTR accelerometer+gyroscope and LIS2MDLTR magnetometer I have to implement an inclinometer and a eCompass with the maximum accuracy. Now, it is not completely clear to me how to g...

MRaff.1 by Associate III
  • 147 Views
  • 0 replies
  • 0 kudos

MotionFx Magnetometer calibration issue

Hello Everyone!!!I am using STM32F401CBU6 controller along with 2 sensors ie., (ISM330DLC & ISM303DAC) in my project. I have included motionfx library and getting Roll, Pitch, Yaw and Heading, but the heading is not getting calibrated and values are ...

FX_Run.PNG Init.PNG Mag_Calib.PNG
Anil3 by Associate III
  • 278 Views
  • 2 replies
  • 0 kudos

Roll value changes with Pitch

Hello Everyone!I am using ISM303DAC sensor in my project and facing an issue with Pitch value.  I have used MotionMC library and  calibrated the Magnetometer for heading. and also it got calibrated. As MotionEC_Run() function output consists of Euler...

Anil3 by Associate III
  • 145 Views
  • 0 replies
  • 0 kudos

Hard Iron Calibration

Hello Everyone!!!I am using ISM303DAC in my project E-Compass, I am facing an issue regarding hard iron calibration. in datasheet it is mentioned that we have do hard iron calibration using external processor  and has to store those values in the int...

ISM303DAC.PNG
Anil3 by Associate III
  • 648 Views
  • 6 replies
  • 0 kudos

clarification regarding sensor orientation

Hi everyone!!!i am working on motionEC library and there i have observed that it need sensor orientation. can anyone explain me what exactly is this orientation meaning and how it effects the library??reagards,regards,ANIL.

Anil3 by Associate III
  • 147 Views
  • 1 replies
  • 0 kudos

LIS3MDL Temperature problem.

Hello. We know that lis3mdl is temperature sensitive, i.e. there is a scale shift. From what we have read, this cannot be compensated for with software ( Or maybe it's possible? ). Therefore, can this be prevented physically, e.g. by using some therm...

TBart.1 by Associate II
  • 217 Views
  • 3 replies
  • 1 kudos