STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1406 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to install (add?) middleware to STM32cubeIDE ?

Hi, Many thanks in advance to help me. And sorry if my question is stupid. I tried to add EEPROM emulation to my NUCLEO Dev board (L476RG). I wasn't able to add this middle ware via the cubeIDE. After that I seen that it is for cubeMX, I tried to but...

dodonny by Associate III
  • 8251 Views
  • 9 replies
  • 1 kudos

C++ code STD::COUT Using STM32CubeIDE 1.5.1 targeting STM32FF746 Nucleo results in a compile error. Hope someone can advice how to solve this.

Middleware used: stm32_usb_deviceLib, freetos, fatfs, lwip. Compiler output: arm-none-eabi-g++ "../SenticsLib/DebugHelper.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DUSE_HAL_DRIVER -D_DEBUG -DSTM32F746xx -DDEBUG -c -I../Core/Inc -I../FATFS/Target -I../F...

schelven by Associate II
  • 1461 Views
  • 0 replies
  • 0 kudos

Resolved! STM32G030K8 Linker-error When I modify the linkerfile for absolute adressing of a variable within the Flash-Memory I get an unexpected Error "FLASH' overflowed by 31912 bytes".

I created a motor control programm for the STM32G030K8 with the MCDSK Software and imported it into the STM32CubeIDE. The programm compiles and works fine on my hardware. When I try to allocate some data on the last 2k Page of the Flash I get an erro...

ASatt.1 by Associate II
  • 2130 Views
  • 3 replies
  • 0 kudos

How to read address in UART in STM32CUBEIDE?

How to read address in UART in STM32CUBEIDE, Actually I am reading RS485 values of Energymeter like Voltage, Current and Power, Energy but I am not able to read the address, also need to know how to read slave id too. Please help me in this regard?

SVerm.3 by Associate III
  • 1153 Views
  • 2 replies
  • 1 kudos

Resolved! How to migrate code from Keil uVision to CubeIDE?

I was able to open the ST25R3911B_DISCO_FW's included DISCO-STM32L4x6.uvprojx file. It builds and debugs easily, until... I try to uncomment back in the functions in its main and while (StreamDispatcherInit, ProcessIO and dispatcherWorker), which th...

Getting hard fault handler issue while running

Hi all,I am working on a project which is based on freertos on stm32l476rg. I have added STM32CubeExpansion_CELLULAR_V5.2.0 into my project and while running I am getting hard fault handler before control comes to main function.These are the remedies...

0693W000008G0jjQAC.png 0693W000008G0lVQAS.png

Resolved! STM32Cube IDE executing commented lines

Hello everyone,I'm debuging a project with 2 recent commented lines, and the debug is executing this lines: I previously builded that project, I don't understand what's happening, maybe you can answer me that question.Thank you in advance!

0693W000008G09WQAS.png
DPrie.1 by Associate II
  • 1750 Views
  • 2 replies
  • 0 kudos