cancel
Showing results for 
Search instead for 
Did you mean: 

SFR Register View for RTC backup registers is using wrong address

WGoeb.1
Associate

Processor: STM32F103

Using the SFR view in STM32CubeIDE, address 0x40006c00 is used for Register DR1;

looking into the software implementation this is actually 4 bytes before the DR1 register, resulting in a shift of DRx register by one.

Also according RM0008 the first 4 bytes based on above offset are reserved.

RN0114 (release notes for STM32CubeIde) are not mentioning this topic.0693W000003PGw3QAG.png

Implementation with HAL (for DR1 value 1 is handed as BackupRegister, resulting in an offset of 4 Bytes) :

uint32_t HAL_RTCEx_BKUPRead(RTC_HandleTypeDef *hrtc, uint32_t BackupRegister)

{

 uint32_t backupregister = 0U;

 uint32_t pvalue = 0U;

 /* Prevent unused argument(s) compilation warning */

 UNUSED(hrtc);

 /* Check the parameters */

 assert_param(IS_RTC_BKP(BackupRegister));

 backupregister = (uint32_t)BKP_BASE;

 backupregister += (BackupRegister * 4U);

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User

Similar: https://community.st.com/s/question/0D50X0000ALwiivSQB/stm32f107-bkp

@Imen DAHMEN​ , can this please be fixed?

Thanks,

JW

Imen Ezzine
ST Employee

Hi,

Thank you for the feedback!

We take note of this and will be fixed asap.

-Imen