STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1405 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

BUGS: Pervasive Dialog Box update issues on Mac OS

There are many dialog boxes within the IDE which do not update properly as you change settings in Mac OS. These include the Manage Configurations dialog, the Symbols tab of the Paths and Symbols dialog box (they don't update as you change configurati...

AVoel.1 by Associate III
  • 1425 Views
  • 2 replies
  • 0 kudos

Installing STM32CubeIDE in Mac OS

STM32 MCUs support,The STM32CubeIDE is installed successfully in Mac OS and it is validated and then it prompts that the software is damaged. I downloaded again and repeat the installation and get same result. How to handle this issue?Best regards,A...

AXu.11 by Associate III
  • 1527 Views
  • 1 replies
  • 0 kudos

How run STM32CubeL4 examples with STM32CubeIDE 1.4.0?

Hi,I´d like run the examples of STM32CubeL4 in STMCubeIDE.In the tutorial "UM1860 User manual", page 17 I read that there´s a directory named "\STM32CubeIDE" with the configuation project to use with STM32CubeIDE. But in the zip file I could not find...

Resolved! "Convert to C++" missing on 1.5.1

I am trying to convert a C project to C++. In the previous version, there was a "Convert to C++" option in the properties. I can't find this in 1.5.1. How to convert to C++ in the new version? Just changing the main.c to main.cpp doesn't do it. ...

JGold.2 by Associate II
  • 4249 Views
  • 10 replies
  • 0 kudos

How do I flash using stlink v3 from Cube IDE?

I currently manage to flash my devices direct from CubeIDE using an stlink V2. However the STM32H7 Discovery board I have has a built in ST-link V3. So how do I flash direct from the IDE WITHOUT having to go through the rather tedious process of ru...

0693W000008GS3MQAW.png
RAshworth by Associate II
  • 1474 Views
  • 0 replies
  • 0 kudos

Resolved! BUG: Display issue on 1.5.1 with Mac Big Sur

First, is this the place to post bug reports for STM32CubeIDE? I'm seeing a few minor bugs but I'll start with this one in case this the right place. A bug was introduced either with a recent release of STM32CubeIDE or with Mac Big Sur. It is hard to...

AVoel.1 by Associate III
  • 2519 Views
  • 4 replies
  • 0 kudos

Resolved! Programming 2 projects at once in STM32Cube IDE

I have 2 seperate projects, the bootloader and the end application.What i want to do is program the bootloader code when i program the application (Run as).I dont need debug capabilities for the bootloader, i just want flash locations 0x08000000 – 0x...

sde c.1 by Senior II
  • 3678 Views
  • 2 replies
  • 0 kudos