STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Multifile search

Hello!It took me a while to figure out how to run a multifile search, and I have questions about it:Is there a way to link the search with ctrl-F like in any other software?What is the search icon supposed to represent? I thought it was the tip of a ...

PG.1 by Associate III
  • 1105 Views
  • 2 replies
  • 0 kudos

B-U585I-IOT02A Discovery Board, USART2 and USART3 Comms

I am trying to use the USART's via the CN2 or CN3 connector.The documentation "um2839-discovery-kit-for-iot-node-with-stm32u5-series-stmicroelectronics.pdf" gives the following pin mappings:CN2USART3_TX -> PD8USART3_RX -> PD9CN3USART2_TX -> PA2USART2...

DWell.1 by Associate
  • 1943 Views
  • 2 replies
  • 0 kudos

FreeRTOS Debug windows not displaying proper data

I have followed the FreeRTOS API document below I have mentioned the details about the documents.FreeRTOS on STM32 CMSIS_OS APIT.O.M.A.S – Technically-Oriented Microcontroller Application ServicesVersion: v1.7Link for document: https://raw.githubuser...

0693W00000QNAPuQAP.png 0693W00000QNAMgQAP.png
HPate.10 by Associate III
  • 8561 Views
  • 11 replies
  • 1 kudos

STMH747 and STM32CubeIDE: how to use USB HOST?

UPDATEToday, as the first thing in the morning I run my USB test that didn't work the last 3 days. Out of the blue it started to... kind of work. The device (USB disk) is detected as mass storage device, so the USB host enters the HOST_CLASS state, t...

HTD by Senior III
  • 4728 Views
  • 2 replies
  • 0 kudos

Issue with fmount / SD Card / SPI /(freertos+fatfs) (Any help would be appreciated) (apparently the sd card is not detected by the NUCLEO_F767ZIT)

in fact i m trying to read and write data on SD card through an adpter using FREERTOS ,spi and fatfs .I m using stm32F767ZIT6the debugger return FR_OK for f_mount when it s put with 0 option and not working for 1 option.the prblms is that even when i...

hMasg.1 by Associate
  • 1655 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeIDE 1.7.0 Clean Project problem (possible BUG)

I noticed a problem (possible BUG) with the Clean Project when working with bigger projects in STM32CubeIDE 1.7. When I try to clean project i get error: make -j12 clean  make (e=206): The filename or extension is too long. make: [makefile:169: clean...

JureL by Senior
  • 5041 Views
  • 6 replies
  • 0 kudos

Resolved! Determine heap free space on STM32

I'm using an STM32L4 with STM32CubeIDE, bare metal, and using C++ along with Cube's C libraries. The compiler is the GCC/G++ supplied with STM32CubeIDE.I have some dynamic memory usage in STL containers etc. I'm aware of the recommendation not to use...

SL-STPM-3PHISO Demo firmware on STM32CubeIDE

Hello,Looking for a free solution to make development for metering, I would like to know if the demo firmware of SL-STPM-3PHISO exists for STM32CubeIDE ?When downloading the proposed solution it seems to be available only for IAR worbench.

EAlir.1 by Associate
  • 804 Views
  • 0 replies
  • 0 kudos