STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 561 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Problem with memcpy

Hello,I am having a problem with simple line of code. If I run code bellow, the result seems off.//Main job of this code is to tranform hex into float uint32_t hex = 0x3fc51eb8; float f; memcpy(&f, &hex, 4);If i go into Live Expressions i g...

GHrib.1 by Associate III
  • 2503 Views
  • 2 replies
  • 0 kudos

Using STM32CubeIDE in order to program SPI1 on STM32U585AII6Q with SW NSS. The relevant pins are not initialized and PinOut seems weird.

Trying to configure SPI1 with SW NSS on STM32U585AII6Q with STM32CubeIDE.While generating the code, the relevant 4 pins are not initialized.The PinOut looks like that. This grey shade seems suspicious to me.Below, MX_SPI1_Init() and MX_GPIO_Init()sta...

0693W00000YAucvQAD.png
bmn by Associate II
  • 1756 Views
  • 1 replies
  • 0 kudos

Resolved! Nucleo-STM32f030 ADC setup Issues This code only works when I'm debugging step by step. Otherwise, it always sends ADEN low again, which should not happen!!

This code only works when I'm debugging step by step. Otherwise, it always sends ADEN low again, which should not happen!! (Correct sequence: ADEN goes high then ADRDY goes high and both stay high...) (Note both ADEN and ADRDY are low before line 54 ...

0693W00000YAXrPQAX.png 0693W00000YAXsWQAX.png
OSell.1 by Associate II
  • 4160 Views
  • 7 replies
  • 1 kudos

Resolved! What can cause HAL_ADCEx_Calibration_Start() to fail?

Here is the code snippet. HAL_Delay(5000); if (HAL_ADCEx_Calibration_Start(&hadc1,ADC_SINGLE_ENDED) != HAL_OK) { print_debug_str("Did not calibrate right!"); } else { char buf[32]; sprintf(buf,"Calibration Factor: %lu\r\n",ADC1->CA...

KiptonM by Lead
  • 12401 Views
  • 4 replies
  • 0 kudos

Resolved! I try to use pmd-eclipse plug-in (static analysis tool). Plug-in is installed and I added -vm corresponding option in stm32cubeide.ini to define correct jdk version but it still not works

The error message says that this plug in needs jdk 17 : jdk 17 is installed and I have added the option -vm with corresponding path to javaw.exe. Error Message is still present after CubeIDE restart.

DWeya.1 by Associate
  • 1163 Views
  • 1 replies
  • 0 kudos