STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1433 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32F4 Timer Interrupts , mode Slave , Toggle on match

Hello everyone, I'm asking for your advice. I use stm32f429i-DISC1 board with display(I use) , HCLK = 96 MHz , APB1 = 48 MHz..., I start the for example timer_1,  output compare CH1 (output)mode=toggle on match ; ...preload = Enable ... , counter per...

gevmar by Associate III
  • 2698 Views
  • 3 replies
  • 0 kudos

ethernet cannot ping but dhcp assigned an address

I have a custom board that used to work with an older version of CubeMx-generated code, but with recent changes, my board no longer works. I made modifications in ethernetif.c to accommodate the known bug. but the board no longer responds to ping fro...

cleonb322 by Associate III
  • 3406 Views
  • 4 replies
  • 0 kudos

Unable to load the image in the STM32F746G Discovery Board.

Hii,Currently I am  working with the STM32F746G Discovery Board,and I have taken an image in the background, and I have also changed the values repeatedly in foreground through TextArea, while the image is tilting in the background.But it is worked f...

Shivani by Senior
  • 1248 Views
  • 1 replies
  • 0 kudos

Trace SWO output in non-debug mode

I've successfully configured the SWO trace output and read the prints in STM32CUBE IDE -> SWV ITM Data Console. I see these prints are working in debug mode. Do STM32 chip (ARM Core) prints the same in non-debug mode (application mode)? If yes, how t...

VMuth.3 by Associate II
  • 9569 Views
  • 9 replies
  • 1 kudos

Strange situation with Lora WAN commissioning

I have changed Lora WAN commisioning But when I open LoRaWAN_End_Node.ioc the I see completly different settings (and I can't edit EUIs and device address).So, when I will change anything other than LORAWAN and generate code for such change then I mi...

markpow_0-1703021009818.png markpow_1-1703021164600.png
markpow by Senior
  • 725 Views
  • 0 replies
  • 0 kudos