STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1422 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32H7 with W5500 SPI DMA not working

My project requires me to make W5500 driver for ethernet. Everything works fine when using non-DMA. But as need to large data continuously, non-DMA is not ideal and need speed thus plan to use SPI DMA with W5500. In past, I had made successfully run ...

jain2051 by Associate
  • 3670 Views
  • 2 replies
  • 0 kudos

Resolved! ADC multi channel configuration(STM32F410)

Hello,I'm using STM32F410 for ADC in which i have configured two channels means two conversions.For IN7 channel the input voltage is 1.89V and for IN8 input voltage is 2.0v(This channel we have connected trimpot voltage can varied ) Please  check the...

Advance_tech_0-1702636700536.png Advance_tech_1-1702636828356.png

Resolved! STM32CubeIDE cannot find OpenSTLinux

I've set up the development environment for an STM32MP157F-DK2 kit including STM32CubeIDE. I'm following instructions to create a new application to run on the A7 under Linux, and CubeIDE cannot find the OpenSTLinux plugin. So I followed the instruct...

Bryan_H by Associate
  • 3210 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeIDE 1.14.0 on Sanoma MacOS fails to open project

Hii, I installed the new version of the IDE 14.1.0, my operating system is macOS Sanoma 14.3. It installed normally, it created a new workspace for me, but when I want to import my projects the program closes, a summary of the system appears to send ...

CColo.2 by Associate III
  • 2377 Views
  • 4 replies
  • 2 kudos

STMCube32IDE importing STM32U5 examples

How do I import the BSP and OSPI_NOR_MemoryMapped examples from the STM32CubeU5 package for the STM32U5A9J-DK board?  That series of board is not listed as supported in the example selector, so I have to use the git repo.  These are all examples that...

boxtor by Associate II
  • 2159 Views
  • 3 replies
  • 0 kudos