STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1553 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Unable to debug from STM32CubeIDE

Hi,I am having a problem where I am unable to run my code in debug mode from within STM32CubeIDE v1.15.I can program the device fine with STM32CubeProgrammer, but when I try to debug I get this output:log output file: C:\Users\[me]\AppData\Local\Temp...

TomC1 by Associate III
  • 4638 Views
  • 7 replies
  • 2 kudos

STM32CubeIDE V1.15 ST-Link upgrade problem

Hi all,I have a STM32C011 project. I am using a STMF0-Discovery as a ST-Link, as I have done many times before.I have upgraded STM32CubeIDE to V1.15. It is asking me to upgrade the firmware in the ST-Link. Going through the upgrade process, it fails ...

PGump.1 by Senior III
  • 15926 Views
  • 15 replies
  • 7 kudos

printf SWO, stlink

Hello everyone,I program on stm32h757 with stm32cube IDE on macOS Sonoma. (stlink v3 minie)Until recently, I debugged with the st link and displayed printf in the swv console without any problem.For technical reasons, I made the program work with the...

Capture d’écran 2024-04-08 à 17.33.37.png
MA4 by Senior
  • 4249 Views
  • 5 replies
  • 0 kudos

Resolved! How to Install STM32CubeIDE Without Internet?

HelloI am a STM32CubeIDE user. After installing STM32CubeIDE for the first time, run it to create a project, you will be prompted to connect to the Internet to download the package as shown in the picture below.However, I need to participate in the c...

0693W00000KcqEpQAJ.png

USB communication

I am Using STM32h563ZIT6 Nucleo Board ,we are not able  serial communicate via USB with other host and with other terminal ,what may be the reason and What are all the configuartion , that we need to set-up before building a code in Cube ide 

ADC - 4 channels crostalk

Hi, im using NUCLEO-u575zi-q and im trying to sample signal via adc multi-channel, im also using DMA to transfer the sampled data into memory buffer. the buffer is filled by this order: in the 0th place of the buffer - channel 1, 1th place of the buf...

Ditzhak by Associate III
  • 2562 Views
  • 3 replies
  • 2 kudos

STM32CubeIDE editor little issue

Hello everyone,I would like just to report a little issue in syntax coloring and self completion in STM32CubeIDE editor.The problem happen when I declare a new function pointer using the typedef:// Request handler function pointer: typedef b08t (*pfH...

iTTy_0-1712823000689.png
iTTy by Senior
  • 911 Views
  • 0 replies
  • 0 kudos

STM32L0 OTA failure

Hi ST experts,I am using the AT command code from ST on the B-L072Z-LRWAN1. I have loaded the bin into the B-L072Z-LRWAN1 via ST-LINK3 switch on the RS232 @ 9600 and get the terminal screen with the AT command working very well. I have a KERLINK gate...

STLearner by Associate III
  • 2896 Views
  • 4 replies
  • 0 kudos