STM32C031G4U6 bare microcontroller with stlink is not detected
i bought 3 STM32C031G4U6 microcontrollers from digikey turkey distributor and soldered them on breakout boards. i have them connected with stlink v2 over SWCLK and SWDIO i double checked connections and power but i can not program them. it just gives out this:
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
what do i do?