STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1406 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

FileX integration with NOR Flash memory

I'm using STM32U083C-DK which has STM32U083MCT6 MCU. And I have an external NOR Flash memory: W25Q32JVSSIQ.I've implemented the SPI communication with the Flash memory and able to reset, read the device ID and do basic Flash memory operations such as...

RB4020 by Associate II
  • 1687 Views
  • 0 replies
  • 0 kudos

How to configure debug for JLink using flash banks?

Hello, I am working with an STM32U5A9NJ, and I have a working elf file that I can load using Ozone. Ozone lets me configure flash banks when I create the project, but it does not seem to have the same feature in STM32IDE. How can I  do this in STM32I...

leofocuy by Associate II
  • 7546 Views
  • 10 replies
  • 0 kudos

Resolved! Not able to program STM32F407VEt6 chip

I built a custom board and attempted to program it using both the ST-Link Debugger V2 and an STM Dongle, but I'm encountering issues and can't seem to program it successfully.Could anyone suggest what the problem might be?

suhas by Associate II
  • 3238 Views
  • 3 replies
  • 0 kudos

Error faced in error handler generated code

Hey! I am beginner with stm32cube ide. I was doing a simple interrupt push button with nvic. I had cross checked all of my initialisations with other posts over here and they matched. I am facing an error while building the project. The error says "e...

beginner_0-1721136300522.png beginner_1-1721136340587.png
beginner by Associate
  • 1611 Views
  • 1 replies
  • 1 kudos

Resolved! smt32cubeIDE opens dual project

I have 2 different projects, different folders, different *.ioc files (project1 and project2)But one of them is related to other one.When I open the project1, the project2 is opens automatically.After that when I closed the project1, the project2 can...

istepne by Associate III
  • 2920 Views
  • 4 replies
  • 1 kudos