STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1406 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Can't find linker flags settings in STM32CubeIDE 1.15.1

Hello,I get this compilation warning: The float formatting support is not enabled, check your MCU Settings from "Project Properties > C/C++ Build > Settings > Tool Settings", or add manually "-u _printf_float" in linker flags.The stated "recipe" to f...

1.png 2.png
JLemi by Associate III
  • 6671 Views
  • 6 replies
  • 0 kudos

I need to integrate the AD7766 library in STM32CubeIDE

Hi STM community,well, i would like to get data from the AD7766 with STM32 via the SPI protocol and I didn't find the AD7766 library to integrate it in the STM32CubeIDE. is there anyone who worked on this before or has a link where i can find the lib...

amlok.1 by Associate II
  • 1875 Views
  • 2 replies
  • 2 kudos

Resolved! C-MACRO in Pre-Build script

Hi, for my STM32CubeIDE projects it would be convenient to have a macro whose value increases every time I compile the project; As if it were a counter of the times I pressed the build button, to be used as an ID to identify the specific build.For ex...

FMass.1 by Associate III
  • 5737 Views
  • 7 replies
  • 2 kudos

include path don't work

Hello, I recently had a compilation error with STM32CubeIDE 1.14.0. A json.h file is not found by the compiler, yet I have included the path in the project properties, as shown in the photo. The file is present in the project/drivers/JSON directory. ...

error.jpg

Resolved! lcd.c file not found

so im trying to run a project example from the stm32h747i disc0 repository from github. specifcally the DCMI project i want to try the camera using snapshot mode or capture mode .when i pen the project and try to build it  i gave this error saying th...

Screenshot 2024-07-05 125336.png
yessine by Associate III
  • 2765 Views
  • 4 replies
  • 1 kudos

STM32G0B1RE USB_DRD_FS

Hi everyone, I am currently working on a project involving the STM32G0B1RE microcontroller and had encountered an issue while configuring the USB_DRD_FS (Dual Role Device Full Speed) in Device mode using STM32CubeIDE.Here are the steps I followed:I s...

sravani by Associate III
  • 14471 Views
  • 34 replies
  • 1 kudos

STM CUBE IDE can not program the board.

Hi All, I am having an issue which is persistent for more than a week. I created a simple blink LED program using STM32 CUBE IDE IDE. I compiled it OK. Then, I tried to run it on the board, CUDE IDE got stuck. I can see from the progress bar that Lau...

stuck_at_initializing.png
demir by Senior II
  • 7842 Views
  • 12 replies
  • 0 kudos