cancel
Showing results for 
Search instead for 
Did you mean: 

Some files popping up

DetlefS
Senior

Hi, I use CubeIDE 12 and compile and load my code with the the green and white 'run debug' button at the top. That works fine but at the end some file from the project pops up and the editor is focus away from the sourcefile to that file. Where/how can I configure this?

THX

Cheers

Detlef 

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
STTwo-32
ST Employee

Hello @DetlefS 

Could you please try to update to last version of the STM32CubeIde.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Andrew Neil
Super User

This is a well-known issue - nothing you can do about it, I'm afraid:

https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-14-0-gt-old-issue/td-p/612850 

https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-opens-random-files-after-run-and-debug/m-p/637754#M24191

https://community.st.com/t5/stm32cubeide-mcus/cubeide-opens-random-files-on-debug-start-end/m-p/593048#M20956

@Souhaib MAZHOUD - any update on that "internal ticket 162500" ?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi, ok, good to know. I only update to a newer version if I'm forced to. Clicking away an unwanted file is too weak a force to update :) .

THX

Cheers

Detlef