STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 561 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Where to report CubeIDE bugs?

Hello,I've updated my STM32CubeIDE to the latest version (1.13.1) and verified that some annoying bugs are still there. I'm curious is there a dedicated place where to report them?I'm talking about really a basic functionality which should be working...

kgardas by Associate III
  • 2792 Views
  • 4 replies
  • 3 kudos

embbeded stm32f746 nucleo board ethernet use

stm32 nucleo board use ethernet communiction  send string on board pb7 led on same off string It looks like you're trying to implement a TCP client on an STM32 Nucleo board that controls an LED connected to pin PB7 based on the string send  on  sever...

Resolved! Problems with Firmware Library Package Setup

Hi,on a brandnew PC with Win10 i installed CubeIDE 1.16.1.After that, i want to import example project "BLE_HeartRate. Then i got this message:  I thougt that CubeIDE installed the required Firmware Package automatically?

2024-10-10_17h49_00.png
ledi001 by Senior
  • 1105 Views
  • 1 replies
  • 0 kudos

regular HAL_RTC WakeUp

Hello,I'm testing the PWR_STOP_RTC sample on STM32L0538-Discovery.I see how to wake-up period with WakeUpCounter in  the function HAL_RTCEx_SetWakeUpTimer_IT().I think I'd generate periodical wakeup interrupt with fixed period.Is  there any specific ...

curiae by Associate III
  • 969 Views
  • 1 replies
  • 0 kudos

Cannot activate IRTIM peripheral

Hi, I'm developing an application based on STM32U031K8. I need to use the IRTIM peripheral to create an IR transmitter. I set TIM15_CH1 and TIM16_CH1 as "Output Compare No Output" but IRTIM peripheral still cannot be activated. May someone help me?

aerauliqa by Associate II
  • 3221 Views
  • 8 replies
  • 0 kudos

Resolved! STM32 cube IDE Debugger error

I have created a demo project using touch gfx I'm able to flash that project using touch gfx. But when I try to flash that project using Stm32Cube ide it raises an error like "Failed to execute M1 command". Please refer attachments for more details.

sai1 by Associate II
  • 4078 Views
  • 5 replies
  • 3 kudos

About Timer work after Stop mode with RTC

Hello,Once I thougt I measure the duration time after entering Stop mode with RTC to wakeup by EXTI interupt on the STM32L0538-Discovery.But I noticed any timers don't work during Stop mode, is this right?And I think after entering Stop mode, any var...

curiae by Associate III
  • 2785 Views
  • 7 replies
  • 1 kudos