2024-06-19 5:03 AM
Hello to everyone,
for my graphical application I usually use custom boards with STM32H750XB mcu.
For all my projects I always used STMCube IDE 1.6.1.
Code is executed from external qspi flash, so I create a bootloader to launch the application and debug it.
Now, I created a new project and I opened it with cube IDE 1.15.1, but I can't debug it.
When external loader finish, and ide shows " Waiting for debugger connection", I get message "failed to insert all hardware breakpoints..." and a break at internal flash address.
It seems, my bootlader doesn't start.
With IDE 1.6.1, after ext loader finishes its work, I can watch on display bootloader screen, and when it jumps to application, debugger links to main app. In 1.15.1, I don't see the booatloader screen.
Thank you
2024-06-24 3:45 AM
Hello @afici ,
Ensure that your debugging tools (such as ST-Link, GDB server) you are using, are up to date.
Did you change the target boot pins?
2024-06-27 3:09 AM
Thank you @Imen.D,
my tools are all up to date.
Can you please tell me where I have to change boot pins?