STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1544 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 586 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! View Src and Inc files in Project explorer

I have read through a couple posts on this but did not get a clear answer.I have two projects in a workspace.  One shows the tree as:  (This is how I want to see it!)The other just shows Core with only .c files.I can't see what is the difference as f...

FJB2069_0-1733868134096.png FJB2069_1-1733868290939.png
FJB2069 by Senior
  • 2064 Views
  • 2 replies
  • 1 kudos

Resolved! Project explorer shows files in two places

in an STM32CubeIDE V1.17.0 project I add folders Application and Application/Src. I add Application/Src to the list of  source locations. I add a couple of new C++ template source files to the Application/Src folder. These compile OK.But why does the...

pde14qro_0-1733479204252.png
pde14qro by Associate II
  • 2779 Views
  • 5 replies
  • 1 kudos

Resolved! application().goToXScreenNoTransition()

Hello, I am having issues in the IDE, with making the application transition screens.What I've noticed is that even though the goToScreenX function for specific screens is declared in the FrontEndApplicationBase.cpp, it hard faults if the screen tran...

Priyank by Senior
  • 997 Views
  • 1 replies
  • 0 kudos

Breakpoint not triggering in STM32CubeIDE

I've got the following interrupt configured for TIM4:void TIM4_IRQHandler(void) { if ( LL_TIM_IsActiveFlag_UPDATE( TIM4 ) ) { LL_TIM_GetDirection( TIM4 ) == 0 ? ++x : --x; LL_TIM_ClearFlag_UPDATE( TIM4 ); } }I know this interrupt is bei...

CTapp.1 by Senior III
  • 1708 Views
  • 2 replies
  • 0 kudos

Resolved! NUCLEO-U083RC SWV issue

Hi,I got an issue where I can no longer activate SWV Viewer option inside debug configuration for my NUCLEO-U083RC board. The SWV checkbox is greyed out. Whether I create a new project or load an existing one, the SWV option is greyed out and can no ...

chris84 by Associate
  • 1623 Views
  • 2 replies
  • 1 kudos